Selecting the RFID Demodulator
Selecting sets the VSA to demodulate RFID modulated signals.
For more information on RFID modulation, see About Opt BHC: RFID Modulation Analysis.
After selecting the RFID demodulator, set the configuration parameters. Select one of the available standard protocol presets or manually set the parameters from the RFID Demod Properties dialog box. See Setting up a measurement for information on how to set up the VSA.
Example recordings
The 89600 VSA includes several example RFID signals that can be used to help you learn how to use the RFID demodulator. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book.
See Also
About Opt BHC: RFID Modulation Analysis