Available Features (RFID)
The standard set of VSA features are applicable to RFID along with the following RFID features:
- Presets for major RFID protocols.
- Support of common RFID modulation formats.
- Generic support for commonly-used line codes.
- Support for time-domain measurements:
- modulation depth
- duty cycle
- rise and fall time
- ripple
Averaging is not available for any demodulated trace data in RFID demod but is applied to numeric error data in the symbol table, as follows:
- rms (video) computes an RMS average from all updates until the measurement is restarted.
- rms exponential is like rms (video) except that averaging continues past the average count with an exponential weighting.
- peak hold/continuous peak hold keeps track of the peak rms error of each update in the table.
- Average Types applicable
to the pre-demodulated spectrum trace data results:
- rms (video)
- rms exponential
- peak hold/continuous peak hold
See Also
About Option BHC: RFID Modulation Analysis
Standard Features and Measurement Capabilities