Inst Spectrum (RFID)
The trace shows the frequency spectrum of the pre-demodulated time data. When RFID Demodulation is enabled, the trace is the averaged, Instantaneous Spectrum display, as shown in the following block diagram. If averaging is off, the and displays are identical.
The trace is derived from pre-demodulated time data, which is 20% longer than the result length.
If averaging is on, the trace does not show the effects of averaging. To see the effects of averaging, use the trace data. See the block diagram below.
The following block diagram shows the VSA signal flow to produce the Spectrum trace:

See Also