Time (RFID)
When RFID demodulation is enabled, the trace shows the time record before digital demodulation. See the following block diagram:
The amount of data included in the trace trace data is a function of the Result Length parameter.
Time trace data and Averaging
trace data is unaffected by time averaging.
See Also
Selecting the RFID Demodulator