CurrentNumAverages
This is a Data Header variable.
Type = Long
CurrentNumAverages is an integer, and indicates the current average counter. It starts at 1 at the start of the average, and goes up to the user-specified number of averages. This variable should be present only when averaging is on, and only on results that have been averaged. For example, it would not be present on the Instantaneous Spectrum.
On an exponential average, the value of CurrentNumAverages goes up to the user-specified number of averages, and then stays at that value for all subsequent scans.
See Also