DataBitOrder

This is a Data Header variable.

Type = int

DataBitOrder specifies the default bit order for symbol table data.

When the Trace > Properties > Digital Demod > Symbol Table Bit Order parameter (which corresponds to the T_DemodTblBitOrder data header) is set to Auto, the symbol table bit order is determined by this parameter.

Each value in the symbol table data is an integer specifying the symbol bits. By default, the bit order for display on the symbol table and in a marker is set to MSB Most significant bit. In a binary coding scheme, the bit having the greatest numerical value. Analogous to the left-most numeric position in a decimal number.-first, but DataBitOrder can be used to specify a different bit order for the symbol table trace and for markers. The possible values and meanings for DataBitOrder are listed below.