T_DemodTblBitOrder

This is a Data Header variable.

Type = Int

T_DemodTblBitOrder specifies the value of the Trace > Properties > Digital Demod > Symbol Table Bit Order parameter that was set for the trace at the time the trace was saved. When the trace is recalled, Symbol Table Bit Order will be set using the T_DemodTblBitOrder data header. The possible values for T_DemodTblBitOrder are listed below.

The T_ variables describe the display setup when the trace was saved. When you recall and display a saved trace, the VSA uses the T_ variables to restore the display settings to their settings when the trace was saved.