DataOverload
This is a Data Header variable.
Type = Boolean
If DataOverload is true, there was an overload detected on the input hardware sometime during the block of time data that was used to produce this result.
There may have been undetected overloads even when this variable is false or not present.