T_DemodCodeOrder
This is a Data Header variable.
Type = Short
T_DemodCodeOrder is the displayed code order for the 3G CDP data: 0 = Hadamard, 1 = Bit Reverse. This is available for both cdma2000 and W CDMA measurements.
The T_ variables describe the display setup when the trace was saved. When you recall and display a saved trace, the VSA uses the T_ variables to restore the display settings to their settings when the trace was saved.