T_DemodTblFormat
This is a Data Header variable.
Type = Short
The value of T_DemodTblFormat indicates whether the Demod Symbol Table is in binary (0) or hexadecimal (1) format.
The T_ variables describe the display setup when the trace was saved. When you recall and display a saved trace, the VSA uses the T_ variables to restore the display settings to their settings when the trace was saved.