TstLim*ResultPoints
This is a Data Header variable.
Type = Boolean Array
In Limit Tests, TstLim*ResultPoints indicates whether the data for each point failed the limit test. The TstLim*ResultPoints array is the same size as the limit tests arrays TstLim*X and TstLim*Y.
The '*' in TstLim*ResultPoints indicates the limit test number, the first limit test being 1 (i.e. TstLim1ResultPoints, TstLim2ResultPoints and so on).