TstLim*X
This is a Data Header variable.
Type = Double Array
In Limit Tests, TstLim*X is one set of X points of the composite limit test. There can be two composite limit tests, one for upper limits and one for lower limits as indicated in TstLim*YSide. This array is the same size as TstLim*Y and TstLim*ResultPoints.
The '*' in TstLim*X indicates the limit test number, the first limit test being 1 (i.e. TstLim1X, TstLim2X and so on).