XStart
This is a Data Header variable.
Type = Double
XStart indicates the X value of the first point in data (start frequency).
Duration in seconds of the first data point relative to the T=0 location
For trace data, XStart may have units of either Points or Sec, which is indicated by the value of XUnit.
XStart is not used for segmented capture.
See Also