TimeSec
This is a Data Header variable.
Type = Double
The value of TimeSec relates the t=0 point of the trace to another point in time, and depends on the Data Source setting when the data was acquired.
- From Recording: offset from the t=0 time of the recording (TimeStamp)
- From Hardware: offset from the t=0 time of the data of the first measurement after measurement restart
See Also