YUnitRelCarrier
This is a Data Header variable.
Type = Boolean
YUnitRelCarrier indicates whether the y-axis units are displayed as relative to the carrier. This is used by Phase Noise Spectrum traces.
-
TRUE: when YUnit is empty or equal to "/Hz", a "c" is put into the unit when showing the trace in the Log Mag format.
Example: YUnit = "/Hz", then in Log Mag the unit becomes "dBc/Hz amplitude in a 1 Hz bandwidth relative to the carrier", rather than just "dB/Hz".
-
FALSE: do not modify y-axis units