About Overall Error Summary Data (TD-SCDMA) Overall Error Summary Table
When TD-SCDMA Demodulation is enabled, table provides error and summary data for individual timeslots within the measured burst.
The available Overall Error summary data includes: DwPTS Phase Coding information and individual timeslot error data which includes Chip Timing, Total Power, Midamble Power and Data field Power error information.
Additional Error Summary Data
TD-SCDMA demodulation also provides these additional Error Summary data tables:
- Channel Error Summary table provides error data for an individual code channel and layer for a specified timeslot and sub-frame.
- Composite Error Summary table provides error data for the composite signal for a specific timeslot and sub-frame.
Querying summary table data results programmatically
To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.
See the How To Query Summary Table Data Results topic for more information.
See Also