Filtered Time (TD-SCDMA)
When TD-SCDMA demodulation is enabled, the Result Length parameter determines the amount of time data that is analyzed and displayed.
trace shows the pre-demodulation filtered time record data. TheOverall
data is unaffected by time averaging.VSA signal flow (see Digital Demodulation Block Diagram):
Display Format
The data is shown in a multi-color alphanumeric format that identifies the detected active timeslots within each measured sub-frame including the uplink and downlink pilot timeslots. The active Marker timeslot used for data analysis is also highlighted. The colors can be changed and redefined using the Display Preferences Color tab.
See Also