Result Length, Start Boundary and Analysis Parameters (TD-SCDMA)
(See TD-SCDMA Standard Setups/Presets Table.)
The Result Length, Start Boundary, Analysis Sub frame, and Analysis Timeslot parametersneed to be specified to completely define the region of the TD-SCDMA frame that is demodulated and analyzed.
determines the signal capture length in terms of sub frames. This is the data used by the VSA for demodulation and signal analysis. Make sure that the result length is long enough to capture all the desired data.
specifies when to start the data capture. The can be specified as Sub-frame or 2 frames (see Selecting a Start Boundary below):
Starts the result length data capture at the first demodulated sub-frame.
: Starts the results length data capture at even numbered frames.
The VSA acquires enough data to ensure that the and the specified data will be captured.
specifies which sub-frame, within the acquired is used for analysis and trace data measurement results. The available selections include the acquired sub-frames.
specifies which sub-frames timeslot, within the selected , is used for analysis and trace data measurement results. The available selections include timeslots 0 through 6, the DwPTS and UpPTS timeslots.
Selecting a Start Boundary
To automatically specify the and information, use the marker feature: from the Overall Time trace data display, simply right click on the trace display and select .
Data Analysis Example
The following example shows how to set the , , and parameters to specify timeslot 3 in Sub-frame number 1 as the :
Start Boundary = Sub-frame
Result Length = 2 Sub-frames
Analysis Sub-frame = 1
Analysis Timeslot = TS3.
Using Triggered Measurements
When making triggered measurements, the demodulation algorithm requires some amount of data prior to the beginning of the desired sub-frame, in order for demodulation to begin on that sub-frame. This is handled internally but if there are delay differences between the sub-frame boundary in the incoming signal and the trigger then the may need to be adjusted in order to supply enough data before the beginning of the sub-frame. For instance, if an external trigger occurs 20 us after the beginning of the desired sub-frame then would need to be set to -20 us.
See Also