ACP PvT Tab (TEDS Demod)
The tab of the TEDS (TETRA2) Demod Properties dialog box lets you access the ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. PvT parameters of the TEDS Demodulator.
The tab dialog box allows you to configure these parameters:
See Also