ACP Bandwidth (TEDS)
18kHz (See Using Standard Setups/Presets)
1kHz to 1/2 Frequency Span
specifies the bandwidth for the ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. PvT analysis measurement filter.
The adjacent channels for ACP PvT tests are configured by specifying an ACP Offset and then a bandwidth around the offset center frequency.
See Also