Extend Frequency Lock Range (TEDS)
Selected (See Using Standard Setups/Presets)
, when selected, increases the frequency lock range by an additional +/-20kHz.
This is a control parameter for modulation analysis that allows an increase in the frequency lock range, within which you can analyze a TEDS signal by an additional +/-20kHz. Clear this check box only in special cases when specific data patterns are causing display instabilities.
See Also