Using Standard Setups/Presets (TEDS)
Click the button to choose from the following preset standard formats:
- Normal Uplink (25kHz, 50kHz, 100kHz, 150kHz)
- Normal Downlink (25kHz, 50kHz, 100kHz, 150kHz)
- Random Access (25kHz)
- Control Uplink
(25kHz, 50kHz, 100kHz, 150kHz)
The Channel Bandwidth needs to be selected before the button is clicked. The preset parameters, including frequency span, ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. Offset, and ACP Bandwidth, are specific to the selected channel bandwidth (as well as the selected slot format).
Some parameters may need to be changed after a Preset to Standard, for example, .
Preset to Standard - Normal Uplink
After selecting Preset to Standard - Normal Uplink, the analyzer automatically enters the TEDS demodulation parameters appearing in the following table:
|
Parameter |
Channel Bandwidths |
|||
|---|---|---|---|---|
|
25kHz BW |
50kHz BW |
100kHz BW |
150kHz BW |
|
|
.35 |
.35 |
.35 |
.35 |
|
|
18kHz |
18kHz |
18kHz |
18kHz |
|
|
25kHz |
37.5kHz |
62.5kHz |
87.5kHz |
|
|
-4 |
-4 |
-4 |
-4 |
|
|
1 |
1 |
1 |
1 |
|
|
selected |
selected |
selected |
selected |
|
|
.2 |
.2 |
.2 |
.2 |
|
|
75kHz |
100kHz |
150kHz |
200kHz |
|
|
cleared |
cleared |
cleared |
cleared |
|
|
selected |
selected |
selected |
selected |
|
|
selected |
selected |
selected |
selected |
|
|
selected |
selected |
selected |
selected |
|
|
cleared |
cleared |
cleared |
cleared |
|
|
16QAM |
16QAM |
16QAM |
16QAM |
|
|
selected |
selected |
selected |
selected |
|
|
55mSec |
55mSec |
55mSec |
55mSec |
|
|
0 |
0 |
0 |
0 |
|
|
1 |
1 |
1 |
1 |
|
Preset to Standard - Normal Downlink
After selecting Preset to Standard - Normal Downlink, the VSA automatically enters the TEDS demodulation parameters appearing in the following table:
|
|
Channel Bandwidths |
|||
|---|---|---|---|---|
|
25kHz BW |
50kHz BW |
100kHz BW |
150kHz BW |
|
|
.35 |
.35 |
.35 |
.35 |
|
|
18kHz |
18kHz |
18kHz |
18kHz |
|
|
25kHz |
37.5kHz |
62.5kHz |
87.5kHz |
|
|
-4 |
-4 |
-4 |
-4 |
|
|
1 |
1 |
1 |
1 |
|
|
selected |
selected |
selected |
selected |
|
|
.2 |
.2 |
.2 |
.2 |
|
|
75kHz |
100kHz |
150kHz |
200kHz |
|
|
cleared |
cleared |
cleared |
cleared |
|
|
selected |
selected |
selected |
selected |
|
|
selected |
selected |
selected |
selected |
|
|
selected |
selected |
selected |
selected |
|
|
cleared |
cleared |
cleared |
cleared |
|
|
16QAM |
16QAM |
16QAM |
16QAM |
|
|
selected |
selected |
selected |
selected |
|
|
30mSec |
30mSec |
30mSec |
30mSec |
|
|
0 |
0 |
0 |
0 |
|
|
1 |
1 |
1 |
1 |
|
Preset to Standard - Random Access Uplink
After selecting Preset to Standard - Random Access, the VSA automatically enters the TEDS demodulation parameters appearing in the following table:
|
Parameter |
Channel Bandwidth |
|---|---|
|
25kHz BW |
|
|
.35 |
|
|
18kHz |
|
|
25kHz |
|
|
-4 |
|
|
1 |
|
|
selected |
|
|
.2 |
|
|
75kHz |
|
|
cleared |
|
|
selected |
|
|
selected |
|
|
selected |
|
|
cleared |
|
|
4QAM |
|
|
selected |
|
|
35mSec |
|
|
0 |
|
|
1 |
Preset to Standard - Control Uplink
After selecting Preset to Standard - Control Uplink, the VSA automatically enters the TEDS demodulation parameters appearing in the following table:
|
|
Channel Bandwidths |
|||
|---|---|---|---|---|
|
25kHz BW |
50kHz BW |
100kHz BW |
150kHz BW |
|
|
.35 |
.35 |
.35 |
.35 |
|
|
18kHz |
18kHz |
18kHz |
18kHz |
|
|
25kHz |
37.5kHz |
62.5kHz |
87.5kHz |
|
|
-4 |
-4 |
-4 |
-4 |
|
|
1 |
1 |
1 |
1 |
|
|
selected |
selected |
selected |
selected |
|
|
.2 |
.2 |
.2 |
.2 |
|
|
75kHz |
100kHz |
150kHz |
200kHz |
|
|
cleared |
cleared |
cleared |
cleared |
|
|
selected |
selected |
selected |
selected |
|
|
selected |
selected |
selected |
selected |
|
|
selected |
selected |
selected |
selected |
|
|
cleared |
cleared |
cleared |
cleared |
|
|
16QAM |
16QAM |
16QAM |
16QAM |
|
|
selected |
selected |
selected |
selected |
|
|
35mSec |
35mSec |
35mSec |
35mSec |
|
|
0 |
0 |
0 |
0 |
|
|
1 |
1 |
1 |
1 |
|
See Also