Loading a TEDS Demo Signal (TEDS)
This procedure shows you how to load a TEDS demo signal: Normal Downlink, 25kHz, 16QAM. With this demo signal, you can review the measurement setup and experiment with the VSA settings, and then adapt the settings to your actual TEDS signal.
-
Preset the 89600 VSA by clicking
-
From the Menu bar, select .
-
Navigate to the demo file: %ProgramFiles%\89600 VSA Software <ReleaseVersion>\89600 VSA Software\Help\Signals\TEDS\TEDS_NUB_50k_16Q.sdf
This is a recording of TEDS Normal Uplink slot format, 50kHz channel bandwidth, and Modulation Type 16QAM
-
Click
-
Click the button for the recording (far-left icon on the VSA toolbar).
You can use the toolbar to select operations such as , , or .
To configure the 89600 VSA at the same time as recalling the demo signal, use the feature instead.
See Also