Measurement Errors
Measurement error messages appear in an error dialog box.
For source (signal generator) errors, see Source Error Messages.
|
|
Measurement error dialog box. The current hardware setup could not acquire enough time samples to complete the requested demodulation measurement. Each demodulation measurement has minimum acquisition requirements specific to that measurement. For example, the Digital Demod Result Length and Search Length algorithms require a minimum of 10 Symbols. This error can be related to the Alias Protect setting for the ESA or Sampling Mode for the Infiniium oscilloscopes and the 6000/7000 Series oscilloscopes (documented in the Infiniium Oscilloscopes with 89600 VSA Software which is listed in the Application and Product Notes topic). |