Inst Spectrum (W-CDMA(3GPP)/HSPA)
(Instantaneous Spectrum) trace data is the non-averaged frequency spectrum of the pre-demodulated Time trace data, where "x" is the VSA input channel number. is the non-averaged trace data.
If averaging is on, the does not show the effects of averaging. To see the effects of averaging, use the Ch1 Spectrum trace data (W-CDMA).
VSA signal flow (see Digital Demodulation Block Diagram):
See Also
VSA Concepts (Windowing and FFTing)