Spectrum (W-CDMA(3GPP)/HSPA)
trace data is the frequency spectrum of the pre-demodulated trace data, where "x" is the VSA input channel number. The data is Windowed (filtered) and FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. performed to create the display.
If averaging is on, trace data is the averaged Instantaneous Spectrum trace data. When averaging is set to zero, the trace data is equal to the trace data.
VSA signal flow (see Digital Demodulation Block Diagram):
See Also
VSA Concepts (Windowing and FFTing)