Composite Phase Error (W-CDMA(3GPP)/HSPA)
Composite Phase Error () is the difference, in phase, between the I/Q reference signal and the I/Q measured signal for composite signal.
The display shows these Phase error values; the RMS (root mean square) Phase Error, the Peak (largest) Phase Error, and the chip number with the Peak Phase Error.
Composite denotes trace data results for the composite signal (includes all Spread Code Lengths (Symbol Rate) and Code Channels).
This parameter is the same as channel Phase error except that the source data is the composite signal. See Channel Phase Error for further information about this parameter.
See Also