Composite Slot (W-CDMA(3GPP)/HSPA)
identifies the first time Slot used in the measurement for the composite signal. The composite Slot ignores the Measurement Offset, which is different than Despread Channel Summary Table Slot data result, which uses the .
See About Measurement Interval and Offset for more information about , , , and interaction.
See Also
Time tab (W-CDMA(3GPP) Demod Properties)