Measurement Offset (W-CDMA(3GPP)/HSPA)
0 Slots (See W-CDMA(3GPP) Standard Setups/Presets Table.)
determines the start position of the Measurement Interval with respect to first Slot within the Result Length. One time Slot is equal to 2560 chips and is equal to 666.7 µs at the default .
and parameters are used to specify what segment of the data is used for data analysis (see About Measurement Interval and Offset).
See Also
About Measurement Interval and Offset