Filter Length (802.11b/g DSSS/CCK/PBCC)
: With first use, 21 chips, otherwise, previous value.
: 3 to 99 chips, odd values only.
sets the filter length for the VSA's equalization filter.
This parameter is available only when the Equalize check box is selected.
Selecting a Filter Length
In general, the best is the smallest that meets your measurement requirements. For measurements at the transmitter, the filter length may only need to be a few chips in length. Longer filter lengths may be needed to measure multi-path environments.
The number of chips determines the maximum filter length that can be entered, as follows:
|
£ [result length] - 2 |
For example, if the result length is 50 chips, the maximum filter length is 47.
See Also
About Equalization (802.11b/g DSSS/CCK/PBCC)
Using Equalization (802.11b/g DSSS/CCK/PBCC)