Automatic (802.11b/g DSSS/CCK/PBCC)
Result Length parameters
result length specifies that the VSA automatically determine the measurement result length. The result length is determined by comparing the input signals chip length to the Maximum Result Length value and using the smaller number.
For more information, see About Result Length.