IQ Offset (802.11b/g DSSS/CCK/PBCC)
IQ Offset (also called I/Q origin offset) indicates the magnitude of the carrier feedthrough signal. When there is no carrier feedthrough, IQ offset is zero (-infinity dB).
IQ origin offset is easily seen in the constellation diagram, as shown below:

In the above illustration, "x" is the center of the constellation diagram. When "x" occurs at the origin, the IQ offset is zero. When "x" is not at the origin, the IQ offset is the magnitude of the vector (in dB) between "x" and the origin.
The carrier feedthrough shown in the symbol table is computed only at the chip times (the instant in time when chips are detected).
See Also