Available Error Summary Data (802.11b/g DSSS/CCK/PBCC)
The following table lists the available 802.11b/g DSSS Direct sequence spread spectrum. The data transmission scheme (sometimes referred to as a "'modulation" scheme) used in 802.11b WLANs. DSSS uses a radio transmitter operating at a fixed centre frequency, but using a relatively broad range of frequencies, to spread data transmissions over a fixed range of the frequency band. 802.11a and 802.11g (when not operating in 802.11b mode) use Orthogonal Frequency Division Multiplexing (OFDM)./CCK complementary code keying/PBCC packet binary convolutional code modulation error data results and PLCP Physical layer convergence protocol Header information.
See About Symbol Table for an overview of the symbol table. Refer to the About Error Summary Data for an overview of the symbol-table error summary data.
|
Available Error Data |
|
|---|---|
For information about using error summary data with ADS, see Demod Errors and ADS.
See Also