Mag Err (802.11b/g DSSS/CCK/PBCC)
Mag Err (magnitude error) is the vector magnitude difference between the I/Q measured signal and the I/Q reference signal at the measured chip time expressed as a percentage of the square root of the mean power of the ideal signal.

The Mag Err data result also provide the chip time with the worst-case peak magnitude error value expressed as a percentage of the square root of the mean power of the ideal signal.
See Also