Status (802.11b/g DSSS/CCK/PBCC)
The status line provides summary messages indicating the status of demodulation of the PPDU 1) IEEE 802.11: PHY (formerly PLCP) protocol data unit or 2) DVB-RCS2 (RLE): payload adapted PDU including the PLCP Physical layer convergence protocol Preamble status, the PLCP Header status and the PSDU 1) PHY Service Data Unit, or 2) PLCP SDU MAC (Medium Access Control: In most wired and wireless networks, a mthod is used to control how and when a device can transmit data over the communications link. This is the network's Medium Access Control scheme. The MAC protocol operates within the Data Link layer (Layer 2) of the ISO OSI 7 layer Model. The IEEE 802.11 standard, for example, specifies the MAC protocol for sharing of the wireless medium, packet formats, addressing, eror detection and recovery following errors. status. The Status message string format is as follows:
[the PLCP Preamble status, the PLCP Header status, the PSDU data status]
- PLCP
Preamble status messages
The PLCP Preamble status indicates whether the SFD Start frame delimiter (Preamble Start Frame Delimiter) was found.
- The SFD (Preamble Start Frame Delimiter) was not found
- The SFD (Preamble Start Frame Delimiter) was found
- PLCP
Header status messages
The PLCP Header status string indicates the status of the PLCP Header:
- Some of the data bits in the PLCP Header were incorrect, but the VSA was still able to determine the data length and data modulation format.
- The header looked correct except for the CRC Cyclic Redundancy Check, which did not match the rest of the header data.
- An extra (incorrect) 90 degree phase shift was detected at the start of the header.
- the detected burst type is 1MB/sec Barker with a short preamble, which is an invalid format.
- means that the result length was not long enough to capture the entire header, so we don't know the status.
- means that the header appears correct and the header CRC passed.
- PSDU
MAC status messages
The PSDU MAC status indicates the status of the PSDU MAC frame.
- If the result length and measurement interval do not contain the entire burst, then this part of the string is left blank
- The PSDU MAC frame check sum fails.
- The PSDU MAC frame check sum passes.
API Programming Information
When queried programmatically, the entry in the summary table is separated into two data results: the HdrStat (PLCP Header status) and MacStat (PSDU MAC status) status information. This table provides the HdrStat and MacStat values and meaning:
|
HdrStat Value |
Description |
|---|---|
|
0 |
No SFD found |
|
1 |
Invalid header bits |
|
2 |
Header CRC failed |
|
3 |
Invalid header phase shift |
|
4 |
Invalid Barker1/short |
|
5 |
Unknown - the result length was not long enough to capture all of the header data, so the status cannot be determined. |
|
6 |
Header OK |
|
MacStat Value |
Description |
|---|---|
|
0 |
Unknown - the result length was not long enough to capture all of the data, so the MAC status cannot be determined. |
|
1 |
MAC FCS Frame check sequence failed |
|
2 |
MAC FCS OK |
See Also