Eq Impulse Response (802.11b/gDSSS/CCK/PBCC)
When 802.11b/g DSSS Direct sequence spread spectrum. The data transmission scheme (sometimes referred to as a "'modulation" scheme) used in 802.11b WLANs. DSSS uses a radio transmitter operating at a fixed centre frequency, but using a relatively broad range of frequencies, to spread data transmissions over a fixed range of the frequency band. 802.11a and 802.11g (when not operating in 802.11b mode) use Orthogonal Frequency Division Multiplexing (OFDM)./CCK complementary code keying/PBCC packet binary convolutional code Demodulation is enabled and the equalizer is ON, the Eq Impulse Response trace shows the impulse response computed from the 802.11b or 802.11g preamble.
For further details, see Using Equalization.
See Also
Ch Frequency Response (802.11b/g DSSS/CCK/PBCC)