IQ Phase Error (802.11b/g DSSS/CCK/PBCC)

When 802.11b/g DSSS Direct sequence spread spectrum. The data transmission scheme (sometimes referred to as a "'modulation" scheme) used in 802.11b WLANs. DSSS uses a radio transmitter operating at a fixed centre frequency, but using a relatively broad range of frequencies, to spread data transmissions over a fixed range of the frequency band. 802.11a and 802.11g (when not operating in 802.11b mode) use Orthogonal Frequency Division Multiplexing (OFDM)./CCK complementary code keying/PBCC packet binary convolutional code Demodulation is enabled, the IQ Phase Error trace shows the error between the I/Q measured and the I/Q reference signals at each demodulated chip time.

IQ Phase Error:

The VSA compares the unwrapped phase, for each chip time, of the I/Q measured signal with the unwrapped phase of the I/Q reference signal. The VSA then displays the phase difference between the two signals.

Phase Drift Compensation

Circular arcs in the constellation of the IQ Meas Time trace display is an indicator of phase drift. The Track Phase demodulation parameter can be used to remove the phase drift, which will improve the IQ constellation trace and reduce the EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. data results (Analysis > IEEE 802.11b/g Demod Properties > Advanced tab > Track Phase check box).

See Also

Available Trace Data (802.11b/g DSSS/CCK/PBCC)

IQ Mag Error (802.11b/g DSSS/CCK/PBCC)