Interpolation Filter (802.11n/ac/ax/be/bn)

The Interpolation Filter parameter applies filtering to the equalizer to reduce signal noise or smooth frequency response.

Equalization values are computed separately for each subcarrier. Since, typically, there is noise on each subcarrier that is independent of noise on other subcarriers, we can average neighboring subcarriers to reduce the noise power in the equalizer response, and consequently, reduce the EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. in the demodulation measurement. This assumes that the true transmitter frequency response is smooth enough, which is usually (though not always) a valid assumption.

However, there is a trade-off: equalizer smoothing makes the equalizer less able to track real frequency-domain roughness in the transmitter, sometimes making EVM worse on signals with low noise or signals with more roughness in the transmitter frequency response.

There are three Interpolation Filter choices:

See Also

802.11n/ac/ax/be/bn Demod Properties

Equalizer Training

Advanced Tab