Advanced Tab (802.11n/ac/ax/be/bn)
The tab of the dialog box configures advanced parameters used to demodulate 802.11n/ac/ax/be/bn signals.
The tab configures these parameters:
- Normalize IQ Traces
- Mirror Frequency Spectrum
- Multi-carrier Filter
- Combine Equalizer using L-LTF
- Compensate Sampling Clock Error
- Compensate IQ Mismatch
- Estimate IQ Mismatch Per Subcarrier
- Decode PSDU and Verify CRCs
- Remove Equalizer Phase Ramp
- Display EVM in Percent
- Display Sync Correlation in Percent
- Subcarrier Spacing
- Subcarrier Spacing (HE/EHT)
- Subcarrier Spacing (Pre-HE)
- Symbol Time Adjustment
- Subcarrier Selection
- Act. Ant. Threshold
- Subcarrier Reference Points Selection
- Spectral Flatness
- SEM Limit Testing
- FFT Length
- FFT Length (HE/EHT)
- Pilot Tracking
- Frequency Estimation Mode
- Equalizer Training
- Channel Estimation
See Also