Decode PSDU and Verify CRCs (802.11n/ac/ax/be/bn)

Decode PSDU and Verify CRCs enables PSDU 1) PHY Service Data Unit, or 2) PLCP SDU decoding and CRC Cyclic Redundancy Check checking. This setting is not available for 802.11ac/ax/be 80+80 mode.

Selected: When selected, PSDU decoding is enabled and CRC verification is performed. When selected, per-user CRC Pass/Fail status and MPDU CRC status are displayed in the OFDM Multi-User Info table. PSDU decoded bits are displayed in the PSDU Decoded Bits trace.

Cleared: (default) PSDU decoding is not enabled and CRC verification is not performed. When cleared, "***" appears in the CRC and MpduCrcStatus columns of the OFDM Multi-User Info table.

For TB PPDUs, the following parameters must be specified for correct decoding:

See Also

Advanced Tab

802.11n/ac/ax/be/bn Demod Properties