Frequency Estimation Mode (802.11n/ac/ax/be/bn)

Frequency Estimation Mode controls which portion of the analyzed 802.11n/ac/ax/be/bn signal will be used for the frequency estimation.

Preamble Only - Only the preamble is used for frequency estimation.

Preamble & Pilots- The preamble and pilots are used for frequency estimation.

Preamble, Pilots & Data - The preamble, pilots and data symbols are also used for frequency estimation.

Default: Preamble Only

See Also

Track Phase

Advanced Tab

802.11n/ac/ax/be/bn Demod Properties