Mirror Frequency Spectrum (802.11n/ac/ax/be/bn)

Mirror Frequency Spectrum enables correct demodulation of frequency spectrums that are mirrored (flipped) about the center frequency. The default frequency spectrum is not mirrored. This parameter does not change the displayed pre-demod spectrum trace data.

Cleared: Does not mirror the frequency spectrum.

Selected: Mirrors the frequency spectrum about the VSA's center frequency.

The display of the pre-demod spectrum data will not change with this parameter. To mirror the pre-demod spectrum, clear the Mirror Frequency Spectrum check box here and select Analysis > Frequency > Frequency tab > Mirror Frequency check box.

External Down Converter

When using an external down converter, specify the User Correction Spectrum "Normal" parameter and make sure the "Mirror Spectrum" parameter is not selected (Input > User Correction > Spectrum > "Normal") and use the Mirror Frequency parameter in the MeasSetup Frequency dialog box instead (MeasSetup > Frequency > Mirror Frequency).

See Also

Mirror Frequency (Meas Setup)

Advanced Tab

802.11n/ac/ax/be/bn Demod Properties