Allocation Mode (802.11n/ac/ax/be/bn)

Use the Allocation Mode radio button to select between per-user RU/MCS modulation and coding scheme/coding setup and simplified setup.

Legacy – existing per-user RU/MCS/coding setup (default, unchanged behavior).

Variant User Info – simplified setup using the 40-bit Variant User Info field from the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.11 standard. Although multiple users can be defined in a Trigger Frame, only one user is supported.

Variant User Info mode is currently only supported for 802.11bn with distributed RUs. The control is grayed out otherwise.

See Also

Format tab

802.11n/ac/ax/be/bn Demod Properties