Standard (802.11n/ac/ax/be/bn)

The Standard drop-down list specifies the demodulator standard format. Standard formats available are listed in Using a Standard Setup. These standards conform to the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.11n-2009 HT high throughput PHY Physical Layer Specification and IEEE P802.11ac/D2.0 VHT very high throughput (VHT) physical (PHY) layer protocol data unit (PPDU):A PPDU transmitted using the TXVECTOR FORMAT parameter equal to VHT. PHY Specification.

The Standard property only configures the demodulator and not the measurement configuration parameters. Use the Preset to Standard button to automatically configure the demodulation parameters.

The 802.11ac 80+80 MHz, 802.11ax 80+80 MHz, 802.11be 160+80 MHz and 802.11be 160+160 MHz selections are only available when the input channel configuration is configured to have 2 measurement channels.

See Also

Format tab

802.11n/ac/ax/be/bn Demod Properties