IQTimeSkew (802.11n/ac/ax/be/bn)

IQTimeSkew is the time difference between the I and Q parts of the signal.

The accuracy of the IQ Impairments, including IQ Gain Imbalance, IQ Quadrature Error and IQ Timing Skew are dependent on the accurate detection of a reference signal.  The accurate detection of a reference signal is dependent on the data modulation format, as well as the cumulative impairments observed during data subcarrier detection.  If the incorrect data modulation format is used, IQ mismatch impairment estimates will be incorrect. 

See Also

Compensate IQ Mismatch (802.11n/ac/ax/be/bn)

IQ Offset (802.11n/ac/ax/be/bn)

IQ Quad Err (802.11n/ac/ax/be/bn)