EVM(w/LO) (802.11n/ac/ax/be/bn)

EVM with LO is the RMS level of the Error Vector Magnitude averaged over all subcarriers including the LO and all analyzed OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbols. EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. is computed in dB.

See Also

About Error Summary Data

Available Error Summary Data