Measurement Interval (802.11n/ac/ax/be/bn)
specifies the time length of Result Length data that is used for computing and displaying the trace data results. is entered as an integer number of OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. symbols. The value must be less than or equal to the parameter.
The parameter combined with the parameter specifies the portion of the result length to analyze and display. The default value is the same as the default . See Measurement Interval and Offset for more information about these parameters and their application.
When the is zero and the is equal to the maximum result length (the default case), changes to the also changes the to match.
See Also