Wireless Connectivity Optional Measurement Software
The following optional Wireless Connectivity modulation analysis measurement software are available for the 89600 VSA software.
-
89601B7RC WLAN WLAN - Wireless Local Area Network: A system that includes the distribution system (DS), access points (APs), and portal entities. It is also the logical location of distribution and integration service functions of an extended service set (ESS). A WLAN system contains one or more APs and zero or more portals in addition to the DS. Modulation Analysis adds the following wireless networking signal analysis capabilities:
-
(89601B-B7R) 802.11a/g/j/p OFDM Modulation Analysis: Orthogonal Frequency Division Multiplexing (OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS.) Vector Modulation Analysis for OFDM standard signals.
-
(89601B-B7R) 802.11b/g DSSS/CCK/PBCC Modulation Analysis: Direct Spread Sequence Spectrum (DSSS Direct sequence spread spectrum. The data transmission scheme (sometimes referred to as a "'modulation" scheme) used in 802.11b WLANs. DSSS uses a radio transmitter operating at a fixed centre frequency, but using a relatively broad range of frequencies, to spread data transmissions over a fixed range of the frequency band. 802.11a and 802.11g (when not operating in 802.11b mode) use Orthogonal Frequency Division Multiplexing (OFDM).) Vector Modulation Analysis for IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org Std 802.11b and for IEEE Std 802.11g standard signals.
-
(89601B-B7S/B7Y) 802.16 OFDM Modulation Analysis: Modulation Analysis for 802.16a-2003 OFDM and 802.16-2004 OFDM standard signals.
-
(89601B-B7Y) 802.16 OFDMA Modulation Analysis: Modulation Analysis for 802.16 Wireless MAN Orthogonal Frequency Division Multiplexing Access signals.
-
- 89601BHXC HT high throughput WLAN Modulation Analysis
- (89601B-BHJ) 802.11n/ac Modulation Analysis: adds wireless LAN Local Area Network: A communications network that serves users within a local geographical area, typically over distances of around 100m. Wireless LANs use wireless communicaitons to network devices so there is no need for data cabling. OFDM-MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. modulation analysis of 802.11n HT and 802.11ac VHT very high throughput (VHT) physical (PHY) layer protocol data unit (PPDU):A PPDU transmitted using the TXVECTOR FORMAT parameter equal to VHT. signals.
- (89601B-BHX) 802.11ax Modulation Analysis: adds modulation analysis of 802.11ax HE signals.
- 89601BHTC IoT Modulation Analysis