Available Trace Data (802.11a/g/j/p OFDM)
The following table provides a list of the available measurement trace data for 802.11a/g/j/p OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. modulation analysis.
OFDM Demodulation |
|
---|---|
See Also
Available Features (802.11a/g/j/p OFDM)