Spectral Flatness (802.11a/g/j/p OFDM)
The parameters specify the data source and limits shown on the Spectral Flatness trace.
Section 1/2, Upper/Lower: defines the minimum and maximum limits of the spectral shape. The exact subcarriers contained by Sections 1 and 2 are defined by the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org standard documents in the Spectral Flatness section. Section 1 can be thought of as the inner subcarriers and Section 2 as the outer subcarriers.
See Also